WHEN.PLFB

Description

Records the value of Position when the when-condition is satisfied. The when-condition is checked once per 250 microseconds.

General Information

Type

R/O

Units

Depends on UNIT.PROTARY or UNIT.PLINEAR UNIT.ACCLINEAR

Rotary: counts, rad, deg, (Benutzerspezifische Einheiten), 16-bit counts

Linear: counts, mm, µm, (Benutzerspezifische Einheiten), 16-bit counts

Range

N/A

Default Value

N/A

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1178

Yes 64 bit Yes

M_01-05-11-000

Related Topics

PL.FB | When